IO-Link as an information channel for Condition Monitoring
IO-Link provides you with real-time status data for your machine. In this white paper, you’ll learn how you can use this intelligent interface to protect your machine from unplanned downtime.
Unlock your knowledge advantage now!
With just a few details, you’ll get access to the selected exclusive content.
IO-Link as an Information Channel for Condition Monitoring
How can machine conditions be made more transparent, maintenance intervals planned more effectively and potential faults detected at an earlier stage? This whitepaper explains the role of IO-Link in the context of condition monitoring, predictive maintenance and Industry 4.0.
The focus is on how information from the machine environment can be used to evaluate plant availability, maintenance requirements and process reliability more precisely. The whitepaper also classifies the key maintenance strategies: from reactive repair and preventive maintenance through to condition-based maintenance using continuous device data.
What You Can Expect from This Whitepaper
The whitepaper explains why end-to-end communication down to the sensor and actuator level is a key element of modern diagnostic concepts. It provides a compact overview of the information IO-Link devices can make available and why this data is relevant for condition monitoring.
Topics covered include:
- the role of IO-Link as an information channel between field devices, controllers, MES, ERP systems and the cloud
- the importance of process data, diagnostic data and device information
- the distinction between device messages, application messages and event messages
- typical information from the machine environment, such as temperature, communication status, operating hours, switching cycles and signal quality
- the relevance of IO-Link in the context of Industry 4.0, condition-based maintenance and predictive maintenance
- the importance of device identification, installation location and function through standardized IO-Link tags
The whitepaper is designed for specialists and decision-makers in automation, maintenance, mechanical engineering and production who want to understand how IO-Link can contribute to machine and plant condition monitoring.
Why This Topic Matters
Rising economic pressure, high availability targets and the need for predictable maintenance are making machine condition data increasingly valuable. Condition monitoring provides the basis for assessing machine conditions not just selectively, but continuously.
IO-Link can help make relevant information from the field level available. The whitepaper does not focus on individual implementation steps. Instead, it provides a clear understanding of which types of data are relevant, which messages can occur and why this information is important for modern maintenance concepts.
Who Should Download This Whitepaper?
This whitepaper is particularly relevant for anyone dealing with:
condition monitoring, predictive maintenance, IO-Link, Industry 4.0, condition-based maintenance, machine diagnostics, sensor technology, automation technology, plant availability and digital maintenance concepts.