skip to main page
Whitepaper

Six criteria for selecting the right UHF RFID tag

How do material, design, temperature, and other aspects of your application influence the choice of the right RFID tag? Use our white paper to find the right RFID tag for your project.

RFID, Track and Trace, Tags HF/UHF

Unlock your knowledge advantage now!

With just a few details, you’ll get access to the selected exclusive content.

How to Select the Right UHF RFID Tag

Choosing the right UHF RFID tag is critical to the reliability and performance of an industrial RFID system. Read range, detection rate, mounting position, environmental conditions and memory requirements all influence whether a tag can be used successfully in a specific application. If the wrong data carrier is selected, objects may not be identified reliably, expected read ranges may not be achieved, or the RFID system may fail to deliver the required performance.

This whitepaper explains what to consider when selecting UHF RFID tags for industrial applications. It focuses on six key criteria that should be evaluated before choosing a data carrier. These include the appropriate frequency range for regional or international use, the material of the object to be identified, the permitted size and position of the tag, and the right tag design for different operating environments.

You will also learn why the surface material matters — including metal, liquids, plastics, wood and textiles — and why certain applications may require specialized RFID tags. The whitepaper outlines the types of requirements that can arise from high temperatures, mechanical stress, protection ratings or exposure to demanding industrial conditions, and explains why these factors are relevant when selecting a suitable UHF tag.

Another focus is on the memory areas of UHF RFID data carriers. The whitepaper describes the basic difference between using a tag for unique identification and using it to store larger amounts of data. It also highlights the questions that should be clarified when deciding whether process-relevant information should be stored directly on the tag or managed in a higher-level system.

The whitepaper also covers RFID tag mounting. Whether a tag is bonded, screwed, embedded, welded or attached with cable ties depends on the application, surface, environment and tag design. The document helps you understand which influencing factors need to be considered before selecting the right RFID data carrier — without revealing the implementation details reserved for the whitepaper.

Download the whitepaper to better assess which UHF RFID tag fits your application and which key questions should be answered before choosing a data carrier.

What you can expect in the whitepaper:

  • The six key criteria for selecting UHF RFID tags
  • An overview of relevant frequency ranges for international RFID applications
  • The impact of material, surface and environment on RFID performance
  • Differences between labels, hard tags and sensor tags
  • Key considerations around memory areas and memory size
  • Important factors for mounting and attaching RFID tags