Klimaatbewaking bij de opslag van soldeerpasta
Turck Beierfeld houdt de klimatologische omstandigheden in de opslagruimte voor soldeerpasta in de gaten met een systeem van het eigen bedrijf – met IM18-CCM50-schakelkastafschermingen, CMTH-sensoren voor conditiebewaking en datadashboards via TURCK Cloud Solutions
Snel te lezen
Voor de elektronica-productie op de vestiging in Beierfeld was TURCK op zoek naar een oplossing om de klimatologische omstandigheden tijdens de opslag en verwerking van soldeerpasta automatisch te bewaken. In de eerste fase van het project werd het eigen IM18-CCM50-platform voor conditiebewaking van het bedrijf gebruikt om continue bewaking van temperatuur, deursluiting en luchtvochtigheid in de koelkasten en soldeerpasta-printers te implementeren. Klimaatgegevens tijdens de verwerking van de soldeerpasta worden nu continu geregistreerd, opgeslagen in de TURCK Cloud en weergegeven op grafische dashboards.
There is a saying that the cobbler's children have no shoes, and the plumber's tap drips. So what about the automation of an automation technology provider? Manufacturers are rarely able to implement every innovation immediately in their own production. After all, new solutions must be tailored to current challenges, and the timing must be right in order to implement new solutions during ongoing operations. At its Beierfeld site, TURCK has now been able to directly implement a recently introduced innovation and automate the handling of solder pastes in electronics manufacturing.
In Beierfeld, the company operates an SMT production facility for printed circuit boards, in addition to many other production lines. SMT stands for Surface Mounted Technology and refers to a production process in which components such as resistors or capacitors are soldered directly onto a printed circuit board – in contrast to the traditional THT (Through Hole Technology) process, in which components with small wire pins are inserted through holes in the printed circuit board and then soldered. In the SMT process, solder paste is applied very thinly (<150 micrometers) to the printed circuit boards by printers. The printed circuit board is then assembled with the components and soldered in the subsequent reflow process.
Climate conditions of solder pastes influence quality
To achieve the best possible solder joint quality, the solder paste must be stored within a specific temperature range. In addition, opened containers may not be used for longer than 30 days. Before processing in the printer, they must be stored at room temperature for at least four hours before the containers may be opened. Following this acclimatization, which prevents condensation, the paste must be mixed for 60 to 90 seconds – shaken, not stirred. On average, the paste may only be processed at 23–27 degrees Celsius – with a humidity of 40–60 percent (depending on the manufacturer). After printing the circuit boards, no more than eight hours may elapse before the circuit boards are soldered in the oven.
All in all, there are a number of parameters that must be adhered to, and manual control of these parameters requires a great deal of attention and care when taking handwritten notes. As with all human processes, there is no such thing as 100 percent certainty when it comes to manual solder paste control. If the specifications are not adhered to exactly, there is a risk of quality losses. The paste then does not optimally fulfill its task of facilitating the melting process and preventing oxidation, resulting in more waste. The production managers in Beierfeld wanted to automate and thus optimize the tracking of solder pastes. Not least within the framework of ISO 9001 and IATF 16949 certification, to which Turck Beierfeld is subject as a supplier to the automotive industry, continuous tracking of processes and preliminary products is mandatory.
Handmatige tracking van soldeerpasta’s
Tot nu toe werden de tijdstippen waarop producten in de koelkast werden geplaatst handmatig geregistreerd door de pastaverpakkingen te scannen. Het uitnemen en openen werd vastgelegd via aantekeningen op de verpakkingen of op documentatieformulieren. De koelkasten beschikten weliswaar al over interne temperatuurmonitoring, maar deze registreerde geen trends; het systeem stuurde alleen een e-mail naar de logistieke afdeling wanneer de temperatuur onder of boven het vastgestelde bereik kwam.
Samen met zijn team en projectmanager Linda Galle heeft Christian Seliger, die verantwoordelijk is voor de afdeling Onderzoek en Ontwikkeling op de locatie Beierfeld, de geautomatiseerde registratie en documentatie van de verwerking van pasta gepland en geïmplementeerd. „Om het project ook tijdens de lopende bedrijfsactiviteiten snel tot een goed einde te brengen, hebben we het project in verschillende fasen opgedeeld”, zegt Linda Galle. „Met onze Plan-Do-Check-Act-aanpak zorgen we ervoor dat elke fase succesvol wordt afgerond voordat de volgende wordt gestart.”
In de eerste fase bestond de eerste taak uit het monitoren en centraal vastleggen van de klimaatomstandigheden van de koelkasten, printers en werkstations voor het voorverwarmen. Het systeem moet de juiste meldingen of alarmen genereren wanneer kritieke waarden worden bereikt. In de volgende fase van het project moeten RFID-ondersteunde registratie van soldeerpasta-blikken en een koppeling met een Manufacturing Execution System (MES) worden geïmplementeerd.
Het klimaat in de koelkasten wordt bewaakt met behulp van het IM18-CCM50-conditiebewakingssysteem van TURCK. Elk van de vijf koelkasten bevat een van deze schakelkastmonitors met een geïntegreerde Linux-computer. De ingebouwde sensoren meten de afstand tot de koelkastdeur en de temperatuur in de koelkast. De apparaten kunnen ook de luchtvochtigheid meten, maar dit is in deze toepassing niet relevant, aangezien er uitsluitend gesloten pasta-verpakkingen in de koelkasten worden bewaard.
De temperatuur en luchtvochtigheid in de printers zijn daarentegen wel degelijk van belang, dus registreert de gecombineerde temperatuur- en vochtigheidssensor CMTH deze variabelen daar. Elk van de drie afzonderlijke soldeerpasta-printers is uitgerust met een van deze sensoren voor conditiebewaking, terwijl een andere sensor de omstandigheden registreert op het werkstation waar de pasta’s worden opgeslagen om op temperatuur te komen. Elke CMTH-sensor is aangesloten op een compacte TBEN-S IO-Link-master, die de gegevens naar het productienetwerk verzendt. De beheerde IP67-switch TBEN-L5-SE-M2 integreert bovendien alle IM18-CCM50's in het productienetwerk.
Met hun open Linux-besturingssysteem zijn de IM18-CCM50 ontworpen voor de installatie van OEM-specifieke software, waardoor gebruikers hun eigen softwareoplossingen kunnen implementeren. Ze vormen het brein van het systeem, dat gegevens opslaat en communiceert met de sensoren, het netwerk en de TURCK Cloud. Voor het monitoren van de koelkasten worden op het conditiebewakingsplatform uitsluitend netwerkstuurprogramma’s en scripts voor het verzamelen van sensorgegevens geïnstalleerd. De IM18-CCM50 verzendt de gegevens van de geïntegreerde sensoren en de CMTH-sensoren rechtstreeks via Ethernet naar de TURCK Cloud.
Overzichtelijke dashboards in de TURCK Cloud geven de weersomstandigheden weer
Deze eerste fase van het project voor het volgen van soldeerpasta zorgt er nu automatisch voor dat de temperaturen in de koelkasten, bij het acclimatisatiewerkstation en in de printers aan de specificaties voldoen. De tijdstippen waarop de pasta’s worden opgeslagen en uitgeslagen, worden momenteel nog handmatig gedocumenteerd of geregistreerd door het scannen van de QR-codes op de verpakkingen. Als de luchtvochtigheid of temperatuur stijgt, kunnen medewerkers dit zien op het dashboard in de TURCK Cloud. Naast de actuele waarden kunnen ook langetermijntrends worden vastgesteld. Trenddetectie en correlaties tussen de gegevensreeksen zouden in de toekomst kunnen worden geanalyseerd door het MES dat nog moet worden aangesloten.
"De nu geïmplementeerde oplossing voor conditiebewaking op basis van de IM18-CCM was slechts de eerste stap op weg naar een volledig geautomatiseerde bewaking van de opslag en het gebruik van soldeerpasta’s. In het vervolgproject zullen we ons MES koppelen en zo de digitalisering en automatisering van onze productie voltooien. Hierdoor kunnen we zelfs bij maximale capaciteit het hoogste kwaliteitsniveau handhaven en onnodige kosten als gevolg van verlopen soldeerpasta's voorkomen”, aldus Christian Seliger, die de tussentijdse resultaten samenvat.
Vooruitzichten: naadloze tracering van soldeerpasta met behulp van RFID
In de tweede uitbreidingsfase zal de tracering van de pasta’s rechtstreeks worden uitgevoerd met RFID-tags op elk blik, waardoor ook de juiste acclimatisatie kan worden geregistreerd voordat de containers worden geopend. Aangezien de IM18-CCM-apparaten vervolgens rechtstreeks communiceren met het MES, dat de productieopdrachten voor de printplaten regelt, kan het systeem onmiddellijk controleren of de gebruikte pastacontainer correct is opgeslagen en geacclimatiseerd voordat de printplaten worden bedrukt, of – in geval van niet-naleving van de voorwaarden – het gebruik ervan blokkeren. Als alle gegevens beschikbaar zijn in het MES, kan daaruit ook aanvullende informatie worden verkregen, bijvoorbeeld om zwakke punten en foutbronnen te identificeren.
Auteur | Klaus Ebinger is directeur Productmanagement Interfacetechnologie bij TURCK