Top ten place at "Germany's best employers"
According to a study by Welt and ServiceValue, TURCK has a "very high attractiveness" and ranks sixth in the industrial sector.
TURCK is once again one of "Germany's best employers." In the latest study by the daily newspaper "Die Welt" in cooperation with the rating agency ServiceValue, the TURCK Group achieved sixth place in the "Industry" category with a value of 2.44.
In the "Germany's best employer 2024" study, 3995 companies from the service, trade and industry sectors are evaluated by around 756,000 citizens in terms of their attractiveness as employers. The survey is conducted without the participation of the companies being evaluated and is based on a population survey on personal perceptions of the image or attractiveness of the employers being examined.