skip to main page
Detection

AI camera enables error-free picking

Using the Difference Check, the TIV AI-based camera reliably detects errors in assembly processes — intuitive commissioning without the need for programming  

Decentralized Automation, IIoT, Smart Cameras

Benefits

  • Easy integration into existing processes without complex programming  

  • AI-based error detection that detects more than the human eye  

  • Fast teaching-in using as few as ten images per status ensures high flexibility when switching products   

  • Clear OK/NOK output and feedback to the PLC  

Challenge

During final assembly at manual workplaces, numerous inspection positions on products often have to be checked. At each position, different statuses can be correct, such as the presence or correct positioning of components. If costly rework and scrappage are to be minimized, the correct placement must be checked automatically during production. It is essential that the complexity of the inspection task does not determine the complexity of commissioning the quality control process. 

Solution

The Difference Check with TURCK Intelligent Vision (TIV) enables teaching-in of objects with several test regions (ROIs). The neural network of the TIV is trained by teaching at least ten images classified as good (OK) and at least ten "incorrect" (NOK) images. The rules behind this are determined by the camera itself. It detects deviations in the test regions and outputs the result via a PLC interface. An image is considered OK if all test regions are correct; otherwise, it is considered NOK. A constant background is essential, as this is also taught in and contributes to object detection. The camera evaluates each test region individually and uses this to determine the overall result. If an issue is identified with a test region, a NOK signal is output that, for example, activates a tower light or triggers the ejection of the product. The personnel are visually informed and can react accordingly.

"TIV makes the difference with its simple commissioning. The camera often knows what is important from just ten images — without the need for time-consuming programming of a set of rules."  

Jannik Suchowitzki | Product Manager Distance Sensors | TURCK GmbH

Experience AI vision live – test TIV now!

Want to know what our intelligent vision solution can really do? Then simply send us some images from your application – our camera experts will analyze your requirements and carry out a free, customized feasibility test with TIV. This will give you a concrete idea of how TIV makes a difference: fast, precise, and reliable.

TURCK1825_pdj_en_Winner

Learn more about our products