skip to main page
Technology

Pick-to-Light

Pick-to-Light systems support manual assembly and order-picking processes through visual user guidance and guided material retrieval

Pick-to-Light

Quick read

Pick-to-Light is a technology that provides visual support for manual assembly and order-picking processes and is used to guide the withdrawal and placement of materials. TURCK’s complete Pick-to-Light solutions support users in manual assembly or order-picking processes with optical guidance. Lights or light curtains—with or without integrated feedback—indicate to the operator which storage bin to retrieve the item from. Depending on the model used, confirmation of the correct withdrawal is either automatic or performed manually by the operator. All components of TURCK’s Pick-to-Light system are designed to work together seamlessly, forming a complete solution for assembly and order-picking tasks. TURCK’s Pick-to-Light systems support installation, operation, and maintenance through their seamlessly integrated system components.

What is Pick-to-Light?

TURCK’s complete Pick-to-Light solutions reliably support users in manual assembly or picking processes. Lights or light curtains—with or without integrated feedback—indicate to the operator which storage bin to retrieve the item from. Depending on the model used, confirmation of the correct withdrawal is either automatic or performed manually by the operator.

All components of the TURCK Pick-to-Light system are optimally coordinated with one another. This allows users not only to install the solution quickly and safely, but also to perform its operation and maintenance reliably.

Benefits

TURCK’s complete Pick-to-Light solutions can be customized using rugged IP67 components. IP20 solutions are also available. Thanks to their high protection rating, the coordinated components can be installed quickly and reliably directly on the equipment. Control cabinets are no longer required.

Customized turnkey solutions can be implemented quickly and cost-effectively thanks to the available hardware and software components. With its experience and the carefully coordinated components of the Pick-to-Light system, TURCK ensures that the entire solution works together seamlessly.

Pick-to-Light in Practice: Added Value for Your Application

Efficient and robust solutions for real-world applications—designed for demanding operating conditions and proven in everyday industrial use.

Pick-to-Light at TURCK: Frequently Asked Questions

1. What is Pick-to-Light, and what is it used for?

Pick-to-Light is a technology that provides visual guidance for manual assembly and order-picking processes. TURCK’s Pick-to-Light solutions use lights or light curtains to indicate to operators which storage bins to retrieve materials from. The technology supports guided workflows in assembly and order-picking applications and, depending on the system, provides automatic or manual confirmation of the withdrawal.

2. How does a Pick-to-Light system work?

A Pick-to-Light system visually guides operators through individual work steps. Pick-to-Light solutions from TURCK use lights or light curtains to indicate the relevant storage bin. The operator retrieves the required material and, depending on the system used, confirms the operation automatically or manually. This allows process control to take place directly at the workstation.

3. What hardware is included in a TURCK Pick-to-Light solution?

Pick-to-Light solutions from TURCK consist of lights or light grids, with or without integrated feedback. The individual components of the system are designed to work together and form a complete solution for assembly and order-picking tasks. The source text describes the hardware as part of a coordinated overall system for industrial applications.

4. What role does Pick-to-Light play in assembly processes?

Pick-to-Light supports assembly processes by providing visual guidance to the operator. TURCK’s Pick-to-Light solutions indicate which storage bin components must be retrieved from. One example of its application is the assembly of subassemblies in the automotive industry, where individual components are provided and retrieved in a specified order.

5. What role does Pick-to-Light play in order-picking processes?

Pick-to-Light supports picking processes by clearly indicating the pickup location. TURCK’s Pick-to-Light systems guide operators step by step through the picking process. One example is material staging in a logistics center, where items are assembled from different storage bins.

6. How does confirmation work in a Pick-to-Light system?

In a Pick-to-Light system, confirmation is either automatic or manual, depending on the model used. TURCK’s Pick-to-Light solutions offer both options. Confirmation verifies that the item has been withdrawn correctly and is an integral part of the guided workflow within the assembly or order-picking application.

7. What benefits does a complete Pick-to-Light solution from TURCK offer maintenance technicians?

TURCK's complete Pick-to-Light solutions consist of components that are designed to work together. According to the source text, this integration helps users with the installation, operation, and maintenance of the solution. As a result, maintenance personnel work with a cohesive system whose components are designed for use together.

8. What software or programming tools are required for Pick-to-Light?

The source text does not mention any software, programming environment, or engineering tools for Pick-to-Light. Pick-to-Light is described as a complete solution with components designed to work together for assembly and order-picking processes. The source does not provide any further details on software functions, licenses, or programming interfaces.

9. What costs or licensing models should be considered for Pick-to-Light?

The source text does not contain any information regarding costs, licensing models, or recurring fees for Pick-to-Light. The source describes Pick-to-Light as a complete solution for assembly and order-picking processes. No further information is provided regarding economic key figures or licensing models.

10. In which industries is Pick-to-Light used?

Pick-to-Light is suitable for manual assembly and order-picking processes across various industries. Examples from the source include applications in logistics as well as assembly processes in industrial manufacturing. A logistics company can use Pick-to-Light for guided order picking, while an automaker can use Pick-to-Light to support assembly processes.