Packaging waste, which has been collected by the Dual Systems in Germany since 1993, ends up in waste sorting plants such as the one in Ochtendung near Koblenz. The disposal company Veolia sorts 90,000 tons of packaging waste every year in this highly automated sorting plant. Packaging that citizens dispose of in yellow bags and bins is separated into a total of 13 different material streams, including main streams of polypropylene (PP), polyethylene (PE) and polyethylene terephthalate (PET), both in film and solid packaging, as well as metal and paper.
Automated precision: How packages are sorted in Ochtende
In the first sorting step, rotating drum screens separate packaging parts from the main flow based on their size. In the end, the entire material, which falls through the last three by three centimeters of sieve openings, is not sorted further and fed into thermal recycling, i.e. burned. In the subsequent sorting process, near-field infrared sensors (NIR) detect different types of plastic and fiber packaging. Magnets and eddy current separators remove ferrous and non-ferrous metals, and so-called wind sifters remove light films by vacuuming.
CIRCPACK by Veolia wants to continuously increase the proportion of recyclable packaging. Since February 2025, the Packaging and Packaging Waste Regulation (PPWR) has been in force, which is intended to reduce the amount of waste through various measures – firstly through recyclable materials, and secondly through the prevention of waste by means of a returnable obligation in certain areas.