skip to main page
Company News

Award-winning TAS software

Turck's IIoT and service platform TAS was "Product of the Year" in the "Software & IT" category

IIoT, Condition Monitoring, Software, TAS

We are delighted by this very special award. Turck products and solutions have received awards time and again. However, the fact that this prize is not awarded by a jury, but by users, in this case the readers of the journal "Computer & Automation", makes it something special. And the fact that first place for "Products of the Year 2024" in the "Software & IT" category goes to a company like Turck, which has traditionally been hardware-driven, clearly shows that we are on the right track with our digital transformation.

The prize went to our IIoT and service platform, TAS — the Turck Automation Suite. The toolset simplifies the management and configuration of Turck devices in industrial Ethernet networks for users. Batch functions, for example, speed up many actions because they can be performed simultaneously on multiple network devices. This saves a great deal of time, for example, during firmware updates or the assignment of IP addresses. Even CODESYS programs can be managed by TAS via the network and easily loaded, backed up, executed and stopped in batch processing. Previously, this had to be done directly in CODESYS on each individual device. TAS also gives users direct access to RFID demo tools and all IO-Link functions of Turck devices, from the IODD configurator to the radar monitor.

We launched the IIoT and service platform a year ago and have been updating it regularly since then. Now we are taking the next big step and adding another module with TAS Cloud.