Condition Monitoring at TURCK: frequently asked questions
What is condition monitoring?
Condition monitoring is the continuous collection and analysis of machine data such as temperature, vibration, pressure, or equipment diagnostics. The goal is to detect wear and deviations early on and prevent unplanned downtime. Condition monitoring provides the data foundation for predictive maintenance.
What is the difference between condition monitoring and predictive maintenance?
Condition monitoring tracks a machine's current condition and flags any deviations. Predictive maintenance goes a step further and uses condition trends to predict when a component is likely to fail. Without condition monitoring, there is no data for predictive maintenance.
Do I need additional sensors for condition monitoring?
In many cases, no. In addition to process values, IO-Link devices also provide diagnostic data such as device status or operating hours, and standard sensors can also serve as data sources when connected to a compatible I/O station. Additional sensors—such as those for vibration—are worthwhile in situations where a specific type of failure would otherwise go undetected.
Does condition monitoring require reprogramming the PLC?
No. At TURCK, status data runs separately from the process control: I/O modules and edge components collect and process it in parallel with the PLC. The PLC application remains unchanged, which is particularly important for existing systems.
Can I retrofit condition monitoring to existing systems?
Yes. Condition data can be collected from existing sensors and IO-Link devices without rewiring the machine or modifying the PLC. This makes TURCK’s approach suitable for both retrofit projects (brownfield) and new machines (greenfield).
What types of data are suitable for condition monitoring?
Typical condition data include temperature, vibration, humidity, pressure, flow, energy consumption, operating hours, switching cycles, and equipment diagnostics. Which of these are relevant depends on the types of failures specific to the application. A good place to start is with the data that existing equipment already provides.
What interfaces does TURCK use to transmit status data?
TURCK transmits status data via open interfaces such as MQTT and OPC UA. The destination can be the TAS Cloud platform, an MES, a maintenance system, or a third-party cloud. In the field, the multiprotocol I/O modules work with PROFINET, EtherNet/IP, EtherCAT and Modbus TCP.
What is ARGEE?
ARGEE is TURCK’s browser-based programming environment for field logic directly within the I/O module. It allows users to monitor limit values, trigger alarms, or preprocess data without placing a load on the PLC or network. For condition monitoring, this means that the I/O module responds to deviations on its own.
When is condition monitoring best performed in the control cabinet, and when in the field?
In the control cabinet (IP20), you can monitor the environment surrounding the control systems—such as temperature, humidity, and door status—using, for example, the cabinet guards from the IMX12-CCM family. In the field (IP67), block I/O modules such as the TBEN collect status data directly at the machine, without a control cabinet. Many systems combine both approaches.
What is the TURCK Automation Suite (TAS)?
The TURCK Automation Suite is a software platform consisting of four modules: TAS Edge for local data processing, TAS Cloud for dashboards, alarms, and remote service, TAS Desktop for device and project management, and TAS Mobile for on-site diagnostics. TAS Edge and TAS Cloud work together primarily for condition monitoring.